Part Number: CC2650
Other Parts Discussed in Thread: CC2531EMK, Z-STACK
Hello,
I am trying to get the SensorTag Z-Stack (Z-Stack Home Automation 1.2.2a) running with a XBee S2C as coordinator module which I have configured to support the HA Profile. Additionally, I am using the CC2531EMK Dongle with the Packet Sniffer application to monitor the ZigBee frames which are exchanged.
Now as far as I can tell from the packet sniffer log the association process after I invoke EZ-Mode by pushing Button SW2 is successful and the green Led starts flashing. But I don't seem to receive the dummy temperature data, which is sent by the SensorTagApp_sendTemp() - Function.
I'm not sure why the communication fails and have attached some screenshots from the sniffer log. I am fairly new to ZigBee and I am not sure what the frames that are exchanged between coordinator and SensorTag mean, maybe these are the Identify Cluster data requests?
This is the successful association:
(1) Association
And after that these packets are being sent:
(2) Data requests
(3a) First part of packets
(3b) Payloads corresponding to the packets from (3a)
Any help is much appreciated! Thanks for your effort!
Cheers,
Felix