Hi, everyone,
I was asked to design a cc2530 with cc2591 front-end PA-LNA system. Meanwhile, I need to use P0.2-P0.5 as a (UART 0, alt 2) debug interface, as I need to connect P1.4-P1.7 (UART 1, alt 2) with hardware flow control to another device. However, it seems to be P1.4 is captured by the CC2591 EN pin, and I can't change the code to let it connect to any other pins. Is there any solution for the P1.4 pin conflict? I'm looking forward for your replies.
Thank you.