This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMARTRF06EBK: SPI Ethernet Module forSMARTRF06EBK

Part Number: SMARTRF06EBK

I should like to  interace an Ethernet Module via the SPI Interface.  We are using the SMARTRF06EBK + CC 2358 and should like to have the device function as a border router in a 6LowPan Mesh Network.  I have looked through the Manuals, but it seems as if  MOSI / MISO  on the board are not  addressable via GPIOs on the CC2358.  Am I missing something.

Regards

Ron