This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2520: CC2520 unexpected connection drops

Part Number: CC2520
Other Parts Discussed in Thread: SIMPLICITI,

Hello, we are facing connection problems with a point to point connection between two CC2520 devices with Simpliciti.

We have an application that is working fine since already long time, but now adding some additional communication traffic, suddenly the connection is dropped from time to time.

Do you have an input what could be the problem and how this could be investigated?

The only error I can see from the master application is the return value from the API “SMPL_SendOpt(..)”, while sending, which returns the error code SMPL_NO_ACK.

If I restart the master without restarting the slave, the connection is working fine again, therefore the slave should still be able to acknowledge the link.

Thanks for help.