This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: OTA upgrade is repeating continuosly

Part Number: CC2530

I have flashed .hex file using CCdebugger in zigbee device and then tried with OTA upgrade with Otaserver tool using (.zigbee file), for first time it is working fine. Then I will be changing output file name in compile options and trying with that file, but OTA file is going upto 100% then again it is starting from 0%. I can't able to find the reason for this. The process is keep on repeating. 

Is there any solution for this issue?