Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK
Hi Team,
I take the default CC2538 End Device example from Z-Stack Home 1.2.2a.
Remove the LCD and LED related peripherals, also set the key as interrupt instead of polling.
Setting poll rate to 10s.
1)
When the CC2538 first time finish the network joining, the current will go to 1.35uA, means the device already get to PM2.
After that, the current will raise up to about 100uA and drop down to 1.35uA again. The procedure took about ~14s.
After that everything works fine.
2)
When reset the CC2538, it will rejoin to the network. Then will see the current raised up again.
From the test, it seems the issue happened when the device first time power up/first time enter to sleep.
Could you help to check why? It should be easily replicated.
Thanks.
Victor Xu