This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Jump to bootloader or erase/write ccfg data?

Part Number: CC2650


We have a device that needs to be switched to serial bootloader mode from the device program (without pressing buttons).

1) Can I go to the bootloader by the jump command to the address? (LDR R0, ORR R0, BX R0)

2) If you can not switch to a bootloader in this way, then, as I know, it is possible to set the word in the CCFG area at CCFG_O_IMAGE_VALID_CONF to a value other than 0x00000000, which means that the firmware will not be validated, and will start the bootloader after restart.
How can I change the value of the CCFG scope?

HWREG(CCFG_BASE + CCFG_O_IMAGE_VALID_CONF) = 0x1; does not work
ti_lib_flash_sector_erase(0x50000000); also does not work.