Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK
Hi,
I am trying to store something to CC2538 Flash at the run time, it's returning nothing and stop working.
The same call I did at start of the Everything, resulting Zero, but After any action it's not working. Please look at my code:
NWK_Bufffer = osal_mem_alloc(64);
printf("22\n");
sprintf(NWK_Bufffer, "%d%d%d", Switch1Sts, Switch2Sts, Switch3Sts);
printf("33\n");
int32_t Res = FlashMainPageErase(KIKO_PAGE_ADDR);
printf("res=%d\n", Res);
ASSERT(Res==0);
printf("44\n");
Res = FlashMainPageProgram((uint32_t*) NWK_Bufffer, KIKO_PAGE_ADDR, sizeof(NWK_Bufffer));
printf("res=%d\n");
ASSERT(Res==0);
printf("55\n");
osal_mem_free(NWK_Bufffer);
Till "33" it's printing, after it's stopping.
Thank you,
regards,
Raghu DS