Part Number: CC2650EM-7ID-RD
Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
Hello,
I have this project of connecting a "ATGM336H" (GPS DEVICE) via the 20pin jtag connectors of the "SMARTRF" CC2650.
However, i do not know or have the required codings to enable the smartrf to:
- Connect to the "ATGM336H" device
- Receive data from the "ATGM336H" collected from the satellite
Are there any project examples regarding connection between CC2650 and an external device (in this case, its GPS receiver)?
My aim here is to connect both of them, and then test it out outside by walking for a few kilometres while the data is collected into the receiver. This probes another question which is, do i need to insert any MICRO-SD into the board since data is being collected?
Thanks.