Part Number: CC2630
Other Parts Discussed in Thread: CC2650
Tool/software: TI-RTOS
It seems that the structs for IEEE commands for the RF core are missing in new releases of TI-RTOS / CC26xxware. You can see the definitions here from an older release. Also, Contiki seems to have a version of the missing header. This is from tirtos_cc13xx_cc26xx_setuposx_2_21_00_06.app (for OS-X) which contains cc26xxware_2_24_03_17272.
The issue came about from generating smartrf settings files that contain IEEE structs such as rfc_CMD_IEEE_RX_t. They do not seem to be defined anywhere in the CC26xxware or TI-RTOS as far as I can tell. Where are these definitions?
Thanks,
Jon