I am trying to build a project utilizing the Zigbee stack, and readily available hardware. I have been looking at the CC2530/31 development kits closely, and have a question about the available inputs. Reading the data sheet on the processor indicates that the ADC on the chip resides on port 0. Looking at the application notes on the development kits hardware seems to indicate that none of the lines from the adc are connected to the SmartRF05 battery board, or the more complex demo board with the attached LCD display. I need access to at least three of the analog inputs to complete my project. Are those inputs made available on daughter board which holds the processor or not?
Any help would be appreciated.
Thanks