Hello, I would like to try to connect via serial via the net-uart. I connected the 6lbr via slip-radio and connected two cc26xx-web-demo nodes. I have enabled the net-uart in project-conf and I saw the IPv6 remote port and the remote port. Now I have connected the two nodes on hercules with two different ports, but writing 1 on com3 i do not get 1 on com2. I also wrote on the linux terminal "nc -6ulkw 1 7777" but nothing.