This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650EM-5XD-RD: what is the difference between CC26XX_PG1 and CC26XX flags in z-stack 1.2.2a?

Guru 14820 points

Part Number: CC2650EM-5XD-RD
Other Parts Discussed in Thread: Z-STACK, CC2530, CC2650, CC2630, CC2538

Hello,

what is the difference between CC26XX_PG1 and CC26XX flags in z-stack 1.2.2a?

  • Hi,

    There are some common files shared between the CC2530/CC2538 and the CC2650 Z-Stack releases, the "CC26XX" compile flag is used to define CC2630/50-only code in these shared files.

    The CC26XX_PG1 compile flag is used for a specific revision of the chip (i.e. PG1.x), this is an old version of the chip so it is likely irrelevant for you. You can check the chip version in Flash Programmer 2.