Part Number: CC2538
Hi,
I am trying to read the data from the NV Memory that I only write. But I was not getting full data please look at my code,
// WRITING //
int32_t nv_length = osal_nv_item_len(KIKO_NV_LAST_STATUSID);
Res = osal_nv_delete(KIKO_NV_LAST_STATUSID, nv_length);
Res = osal_nv_item_init(KIKO_NV_LAST_STATUSID, sizeof(NWK_Bufffer), (uint32_t*) NWK_Bufffer);
NWK_Bufffer = osal_mem_alloc(128);
sprintf(NWK_Bufffer, "1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9");
HalUARTWrite ( MT_UART_DEFAULT_PORT, "Storing Status \r\n", strlen("Storing Status \r\n") );
HalUARTWrite ( MT_UART_DEFAULT_PORT, NWK_Bufffer, strlen(NWK_Bufffer) );
HalUARTWrite ( MT_UART_DEFAULT_PORT, "\r\n", strlen("\r\n") );
Res = osal_nv_write(KIKO_NV_LAST_STATUSID, 0, sizeof(NWK_Bufffer), (uint32_t*) NWK_Bufffer);
ASSERT(Res==0);
Osal_mem_free(NWK_Bufffer);
// READING //
int32_t nv_length = osal_nv_item_len(KIKO_NV_LAST_STATUSID);
Res = osal_nv_item_init(KIKO_NV_LAST_STATUSID, sizeof(NWK_Bufffer), (uint32_t*) NWK_Bufffer);
NWK_Bufffer = osal_mem_alloc(128);
Res = osal_nv_read(KIKO_NV_LAST_STATUSID, 0, sizeof(NWK_Bufffer), (uint32_t*) NWK_Bufffer);
HalUARTWrite ( MT_UART_DEFAULT_PORT, "Reading Status \r\n", strlen("Reading Status \r\n") );
HalUARTWrite ( MT_UART_DEFAULT_PORT, NWK_Bufffer, strlen(NWK_Bufffer) );
HalUARTWrite ( MT_UART_DEFAULT_PORT, "\r\n", strlen("\r\n") );
RESULTS ARE:
Storing Status
1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9,0,1,2,3,4,5,6,7,8,9
Reading Status
1,2,E
Hi Can any one tell why I am not getting all the stored data.
Thank you.