Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Hi. How can I increase the TX power to the max (especially for Beacon Requests) of the CC2530 in SampleLight so it can transmit further? I would really appreciate any help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. For a CC2530, what value should I put inside of macRadioSetTxPower( ? ) to give the maximum TX power?
2. What is the default value inside of macRadioSetTxPower() to begin with?
3. Also if I change the TX power, why do you say there is no way to increase the TX power for the beacon request?