Part Number: CC2538
Other Parts Discussed in Thread: CC2530, CC2531, Z-STACK, CC2650, CC2630
Hi everybody,
I am thinking about starting a new ZigBee project. The platform I finally choose will depend on the answers of the following questions:
- Regarding CC2538, I have read several posts about its high power consumption and few code space (since it has been around some years). Can you confirm that? Also, is CC2538 reaching end-of-life soon?
- Regarding CC265x, is TI's ZigBee stack for this platform as mature as the one for CC2538? Which parts of it are not available for this newer platform when compared to CC2538?
- Finally, is there any existing (or arriving soon) chip, SoC, platform or family from TI that I should consider?
Ok, let's see which are your opinions!
Have a really nice day :)