This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: HSUART configuration

Tool/software: Linux

can any one tell me the configuration for HSUART of termios??.I configured TX,RX,RTS and CTS but still it's not working.

  • /*******************************************************************************
     * @file        : Zigbee_application.c
     * @brief       : Topic :
     *                  This program test for the zigbee application.
     * @author      : Venu (venu.kovelamudi@vvdntech.com)
     * @Copyright   : (c) 2017 , VVDN Technologies Pvt. Ltd.
     *                  Permission is hereby granted to everyone in VVDN Technologies
     *                  to use the Software without restriction, including without
     *                  limitation the rights to use, copy, modify, merge, publish,
     *                  distribute, distribute with modifications.
     ********************************************************************************/
    
    /* Header files declarations */
    #include <stdlib.h>
    #include <string.h>
    #include <stdio.h>
    #include <unistd.h>
    #include <fcntl.h>
    #include <termios.h>
    
    
    /**
     * @funtion : main
     * @brief   : This program sets the configuration of HSUART between MSM8909
     *            and QCA4024. To get the data and send the commands depending on the
     *            user prospective.
     **/
    int main(int argc, char **argv)
    {
        /* structure indicates HSUART configurations */
        struct termios tio, stdio, old_stdio;
        int tty_fd = 0, BAUDRATE = 0;
        unsigned char chp = '\0', cht = '\0';
    
        if (argc != 3) {
            printf("Error:Inavalid arguments\n");
            printf("Usage:./a.out /dev/ttyHS0 B115200\n");
            return EXIT_FAILURE;
        }
    
        /* Get the previous configurations of the terminal */
        tcgetattr(STDOUT_FILENO, &old_stdio);
        /* Clear the structure data for terminal*/
        memset(&stdio, 0, sizeof(stdio));
        /* input modes */
        stdio.c_iflag = 0;
        /* output modes */
        stdio.c_oflag = 0;
        /* control modes */
        stdio.c_cflag = 0;
        /* local modes */
        stdio.c_lflag = 0;
        /* Minimum number of characters for noncanonical read (MIN). */
        stdio.c_cc[VMIN] = 1;
        /* Timeout in deciseconds for noncanonical read (TIME). */
        stdio.c_cc[VTIME] = 0;
        /* TCSANOW -> The change occurs immediately. */
        /* TCSAFLUSH -> The change occurs after all output written to fd has been transmitted.
           This option should be used when changing parameters that affect output. */
        /* Sets the new attributes for terminal */
        tcsetattr(STDOUT_FILENO, TCSANOW, &stdio);
        tcsetattr(STDOUT_FILENO, TCSAFLUSH, &stdio);
        /* make the reads non-blocking */
        fcntl(STDIN_FILENO, F_SETFL, O_NONBLOCK);
        /* Clear the structure data for HSUART*/
        memset(&tio, 0, sizeof(tio));
        tio.c_iflag = 0;
        tio.c_oflag = 0;
        /* 8n1, see termios.h for more information */
        tio.c_cflag = CS8 | CREAD | CLOCAL | CRTSCTS;
        tio.c_lflag = 0;
        tio.c_cc[VMIN] = 1;
        tio.c_cc[VTIME] = 5;
        /* Open the HSUART port for read and write */
        if((tty_fd = open(argv[1], O_RDWR | O_NOCTTY | O_NONBLOCK)) == -1){
            printf("Error while opening\n");
            return EXIT_FAILURE;
        }
        BAUDRATE = atoi(argv[2]);
        /* If the input baud rate is set to zero, the input baud rate will be equal to the output baud rate. */
        cfsetospeed(&tio, BAUDRATE);
        /* sets the input baud rate */
        cfsetispeed(&tio, BAUDRATE);
        /* Sets the new attributes for HSUART */
        tcsetattr(tty_fd, TCSANOW, &tio);
    
        while (cht != 'e' && cht != 'E') {
            /* Read the data from the HSUART */
            if (read(tty_fd, &chp, 1) > 0){
                printf("p%c\n", chp);
                /* if new data is available on the serial port, print it out */
                write(STDOUT_FILENO, &chp, 1);
            }
            /* Read the data from the terminal */
            if (read(STDIN_FILENO, &cht, 1) > 0){
                printf("u%c\n", cht);
                /* if new data is available on the console, send it to serial port */
                write(tty_fd, &cht, 1);
            }
        }
    
        /* Close the file discriptor */
        close(tty_fd);
        /* Sets the old attributes for terminal */
        tcsetattr(STDOUT_FILENO, TCSANOW, &old_stdio);
        return EXIT_SUCCESS;
    }
    

  • I attached the file please check?
  • Couldn't understand you question. Can you elaborate what you are testing?
  • i am checking the High speed uart loopback it's not working, why because configuration is not correct
  • Can you elaborate what host CPU and Zigbee chip you use in this test and what SW do you run on Zigbee chip?