Part Number: CC2530
Other Parts Discussed in Thread: CSD, CC2592, Z-STACK, CC2591, CC2590
Hello everyone,
I am upgrading my project from z-stack2.5.1.a to z-stack3.0.1.
My end device consist of CC2530 + RFX2401.
I am using P1.1(for RXEN) and P1.2(for TXEN).
I did set #define HAL_PA_LNA and In mac_radio_defs.c
if (paLnaChip == PA_LNA_SE2431L)
{
/* CPS or P0_7 maps closely to the HGM line */
HAL_PA_LNA_RX_HGM();
/* EN or CSD line is controlled via software so setting it high here to start the SE2431L frontend */
HAL_PA_LNA_RX_CSD_HIGH();
/* CTX or P1_1 maps closely to PAEN */
RFC_OBS_CTRL0 = RFC_OBS_CTRL_PA_PD_INV;
OBSSEL1 = OBSSEL_OBS_CTRL0;
}
else if(paLnaChip == PA_LNA_CC2592)
{
/* P1_1 -> PAEN */
RFC_OBS_CTRL0 = RFC_OBS_CTRL_PA_PD_INV;
OBSSEL1 = OBSSEL_OBS_CTRL0;
/* P1_0 -> EN (LNA control) */
RFC_OBS_CTRL1 = RFC_OBS_CTRL_LNAMIX_PD_INV;
OBSSEL0 = OBSSEL_OBS_CTRL1;
}
else
{
/* P1_1 -> PAEN */
RFC_OBS_CTRL0 = RFC_OBS_CTRL_PA_PD_INV;
OBSSEL1 = OBSSEL_OBS_CTRL0;
/* P1_2 -> EN (LNA control) */
RFC_OBS_CTRL1 = RFC_OBS_CTRL_LNAMIX_PD_INV;
OBSSEL2 = OBSSEL_OBS_CTRL1;
}
Then I have one issue.
I think that RF Amplifier don't work.
Because I captured packet of coordinator with packet sniffer , LQI of packet is 5 ~ 30.
I attached sniffer log file.
Please help me.
Thanks in advance.
Piao