Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Hello,
I am using Z-Stack 3.0.1 for Home Automation Profile. Here I am doing Permit Join form Z-Stack Linux Gateway which has Z-Stack 3.0.1 ZNP, so when I am trying to add a new device to the network through mesh network I am unable to add it to the network.
I a tried Sniffing the packets, here we can see that the device (that need to join the network) can associate to the respective device which is on the network, but it can not confirm the join in the network.
I have attached the sniffer file, please can anyone help me out here.
Here my Coordinator IEEE Address is 00:12:4B:00:09:DD:6A:97 and the Device that is on the network (through which other device is trying to join the network) is 00:12:4B:00:09:E2:FD:04 and the device that is trying to get in the network is 00:12:4b:00:09:e2:91:6e