This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538-CC2592EMK: Association table size??

Guru 14820 points

Part Number: CC2538-CC2592EMK
Other Parts Discussed in Thread: Z-STACK

Hello,

I am using cc2538-cc2592emk with z-stack 3.0

1) what is the association table size currently defined for coordinator/znp ??

2) what is the max possible size of association table for coordinator/znp and where it is defined /can be modified?

3) what is the association table size currently defined for ZR ??

4) what is the max possible size of association table for ZR and where it is defined /can be modified?