Part Number: CC2538-CC2592EMK
Other Parts Discussed in Thread: CC2592, Z-STACK, CC2538, , CC2531
Hi, I'm developing a Zigbee Hub that uses CC2538 in combination with CC2592. The Software Stack I'm using is Z-Stack Linux. The CC2538 must communicate with my SoC via UART without flow control.
I have a precompiled hex file that kinda works with CC2538 but that doesn't make use of the CC2592 LNA, infact I checked the PA_EN and LNA_EN lines with the scope and both are low, which means the precompiled hex I have is definitely not driving them.
At this point I decided to enable a trial version of the IAR for ARM (8.11.2) and try to compile the ZNP application that comes with ZStack 3.0.1 for CC2538 by myself. Unfortunately when I flash the CC2538 with the latter firmware, ZStack Linux fails completely to communicate with CC2538 ([Z_STACK/LSTN] ERROR : apicSendSynchData() failed getting response).
(Just for reference this is the full path of the ZNP application I'm trying to compile C:\Texas Instruments\Z-Stack 3.0.1\Projects\zstack\ZNP\CC2538, is that the right one for communicating with ZStack Linux?).
Since I want to enable CC2592 LNA and UART communication, I edited the following files:
OnBoard.h (so that compiles with IAR 8.11 as suggested by JasonB)
....
#define CSTACK_BEG ((uint8 const *)(_Pragma("segment=\"CSTACK\"") __segment_begin("CSTACK")))
//#define CSTACK_END ((uint8 const *)(_Pragma("segment=\"CSTACK\"") __segment_end("CSTACK"))-1)
....
OnBoard.c
.... // for (ptr = CSTACK_END; ptr > CSTACK_BEG; ptr--) for (ptr = CSTACK_END, ptr--; ptr > CSTACK_BEG; ptr--) .... //return (uint16)(CSTACK_END - ptr + 1); return (uint16)(CSTACK_END - ptr); ....
hal_board_cfg.h
.... #define HAL_PA_LNA #define HAL_PA_LNA_CC2592 #define xHAL_PA_LNA_CC2590 .... // Values based on powerup h/w config as input with pull-up - not using dynamic cfg of transport. #define ZNP_CFG0_32K_XTAL 1 /* 32kHz crystal installed and used */ #define ZNP_CFG0_32K_OSC 0 /* 32kHz crystal not installed; internal osc. used */ #define ZNP_CFG1_SPI 0 /* 1 */ /* use SPI transport */ #define ZNP_CFG1_UART 1 /* 0 */ /* use UART transport */ ....
MT_UART.h
.... #if !defined MT_UART_DEFAULT_BAUDRATE #define MT_UART_DEFAULT_BAUDRATE HAL_UART_BR_115200 /* HAL_UART_BR_38400 */ #endif ....
flow control should be disabled as ZNP_ALT is defined under the option section (under C/C++ Compiler - Preprocessor) as well as the following:
xHAL_UART_USB xUSB_SETUP_MAX_NUMBER_OF_INTERFACES=5 xHAL_SPI=TRUE HAL_UART=TRUE BDB_FINDING_BINDING_CAPABILITY_ENABLED=0 TC_LINKKEY_JOIN ewarm CC2538_USE_ALTERNATE_INTERRUPT_MAP=1 CC2538ZNP ZNP_ALT xPOWER_SAVING FEATURE_SYSTEM_STATS FEATURE_RESET_MACRO ZDNWKMGR_MIN_TRANSMISSIONS=0 MT_UART_DEFAULT_OVERFLOW=FALSE ASSERT_RESET MAKE_CRC_SHDW SBL_CLIENT ZCL_READ ZCL_DISCOVER ZCL_WRITE ZCL_BASIC
The configuration I'm trying is CC2538ZNP-with-SBL but I've also tried CC2538ZNP-without-SBL without success (haven't tried and CC2538ZNP-Debug yet). What config should I use?
Can you please advise a solution or perhaps provide a precompiled HEX file for CC2538 with UART and CC2592 enabled?
Any help would be very much appreciated.
Thanks,
John