Normal 0 21 false false false DA X-NONE X-NONE MicrosoftInternetExplorer4
Hey,
I was hoping someone could help me here. I'm currently making my final project at my school.
And I'm building a wireless system, and i don't know if the ZigBee can run. I'm currently using the IAR Workbench.
http://en.wikipedia.org/wiki/ZigBee
ZigBee operates in the industrial, scientific and medical (ISM) and 2.4 GHz in m st jurisdictions w rldwide. The technology is intended to be simpler and less expensive than other WPANs such as Bluetooth. ZigBee chip vendors typically sell integrated radios and microcontrollers with between 60K and 256K flash memory, such as the Jennic JN5148, the Freescale MC13213, the Ember EM250, the Texas Instruments CC2530 and CC2520, the Samsung Electro-Mechanics ZBS240 and the Atmel ATmega128RFA1. Radios are also available as stand-alone components to be used with any processor or microcontroller. Generally, the chip vendors also offer the ZigBee software stack, although independent ones are also available.
it says here that ZigBee runs in the industrial, and scientific ... and runs at 868 MHz witch mean that it could run together with the CC1110. but on some of the thinks you can download from texas instrument, it dosen't say that the two things can run together
sorry for my bad english, and hope that someone could help me better undersand this
Best Requards
Marck Hansen