This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: adapt cc2530 code per_test to cc2531

Part Number: CC2531
Other Parts Discussed in Thread: CC2530, Z-STACK

Hi everery one,

I'm trying to adapt the code of the cc2530 per_test from the sdk swrc135b to the device cc2531. The code work fine when read and send the first time then the code stop to read. In the cc2530 work fine the same code. Any can tell what could be happening?  

Regards,

  • Hi,

    You probably need to update the HAL layer with CC2531 board files if you haven't already. You can obtain these board files from the GenericApp project in Z-Stack 3.0.1. In the CC2531 GenericApp IAR project, refer to the files in HAL > Target > CC2530USB