Part Number: CC2538
Other Parts Discussed in Thread: HDC1080
Hi TI Expert Team
I am working on TI CC2538 based 6LoWPAN project, I designed a number of custom board based on CC2538, I have 2 I2C devices on the board ( an EEPROM and HDC1080) , in my earlier boards the I2C used to work fine for read / write both the EEPROM and HDC 1080 without any issue, however in my latest custom board, I2C bus is giving trouble.
There is only a minor change in the bus layout. The I2C bus lines both SDA and SCL are high and i see no transactions when both of the devices are connected ( EEPROM 24C04 and HDC 1080)
.
However if I take out the HDC1080, the EEPROM read write works fine.. my oscilloscope do not have a a i2c bus analyzer and its becoming real difficult to find out the issues. It would be great if you can help me out. I can share all information( board layout , code etc ) if required.
Regards
Kanchan