Part Number: CC2650
Other Parts Discussed in Thread: CC2530
Tool/software: TI-RTOS
Hello,
I am using cc2650 as a Zigbee End-Device based on simplelink SampleSwitch.
When flashing the same project in different custom PCBs produced in the same lot, using maximum available Tx Power, I am seeing that 40% of them have very low LQI and their communication range is below 5 meters where the other 60% of lot can go up to 30 meters without any problems.
Using spectrum analyser I saw that the output frequency of the "bad" PCBs are about 25 ~ 50KHz next to the center channel frequency.
My question is: Is there a way to tune the output frequency in TI-RTOS? In cc2530/31 there is FREQTUNE register that can be modified, but in cc2650 I couldn't find somthing (not even in Smart RF Studio).
Thank you in advance,
Spyros