Part Number: CC2650
Other Parts Discussed in Thread: ADS1220, , Z-STACK
Hi,
i have an issue like an hold post : Syama Sasikumar from Feb 17, 2016 5:49 AM.
It's about an SPI issue with a CC2650 : I want connect on the SPI cc2650 an ADS1220 das.
I use the board-spi.c driver but there is no signal on clock pin.
In the spi_open api, clock pin number is passed as an argument. I have passed my clock pin number as the argument to the function.
Is someone know this issue ?
Thnak's in advance.
Pierre