Part Number: CC2538
Hi everyone! I'm working with CC2538 as i2c master and have a problem with reading bytes from eeprom 24lc16b. This eeprom always responds 0xFF and I don't know why. There are two pull-up resistors 2.5k - on SDA and SCL pins. I attached three oscilloscopes diagrams: first is on writing byte 0x1, second - on sending eeprom address before reading (the same) and third - on reading. My code is here:
//
// The I2C peripheral must be enabled before use.
//
SysCtrlPeripheralEnable(SYS_CTRL_PERIPH_I2C);
//
// Configure I2C pins
//
GPIODirModeSet(GPIO_I2C_BASE, PIN_I2C_SCL, GPIO_DIR_MODE_HW);
GPIOPinTypeI2C(GPIO_I2C_BASE, PIN_I2C_SCL);
GPIODirModeSet(GPIO_I2C_BASE, PIN_I2C_SDA, GPIO_DIR_MODE_HW);
GPIOPinTypeI2C(GPIO_I2C_BASE, PIN_I2C_SDA);
//
// Configure pins as peripheral input and output
//
IOCPinConfigPeriphInput(GPIO_I2C_BASE, PIN_I2C_SCL,
IOC_I2CMSSCL);
IOCPinConfigPeriphInput(GPIO_I2C_BASE, PIN_I2C_SDA,
IOC_I2CMSSDA);
IOCPinConfigPeriphOutput(GPIO_I2C_BASE, PIN_I2C_SCL,
IOC_MUX_OUT_SEL_I2C_CMSSCL);
IOCPinConfigPeriphOutput(GPIO_I2C_BASE, PIN_I2C_SDA,
IOC_MUX_OUT_SEL_I2C_CMSSDA);
//
// Enable and initialize the I2C master module. Use the system clock for
// the I2C module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps. For this example we will use a data rate of 100kbps.
//
I2CMasterInitExpClk(SysCtrlClockGet(), false);
#define I2C_ADDR_24LC16 (0xA0UL)
i2c_addr = (DWORD)((I2C_ADDR_24LC16 & 0xF0)>>1);
//writing
//eeprom address + memory block address. Last param means writing
I2CMasterSlaveAddrSet(i2c_addr|0x1, false);
//put a byte 0x1 to DR register
I2CMasterDataPut(0x1);
//send eeprom address, memory block address and a byte
I2CMasterControl(I2C_MASTER_CMD_SINGLE_SEND);
//wait until done
while(I2CMasterBusy());
//reading
//eeprom address + memory block address. Last param means writing
I2CMasterSlaveAddrSet(i2c_addr|0x1, false);
//send eeprom address and memory block address
I2CMasterControl(I2C_MASTER_CMD_SINGLE_SEND);
//eeprom address + memory block address. Last param means reading
I2CMasterSlaveAddrSet(i2c_addr|0x1, true);
//send eeprom address and memory block address
I2CMasterControl(I2C_MASTER_CMD_SINGLE_SEND);
//read byte from DR register
uint32_t ans = I2CMasterDataGet();
//wait until done
while(I2CMasterBusy());
Writing:
Sending address:
Reading:
Please, help somebody to solve this problem.