This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: No communication between End Device and Coordinator for extended period of time

Part Number: CC2530
Other Parts Discussed in Thread: CC2531,

Hi,

I have been running multiple end device modules for a day, and I am testing if the end device will still be able to communicate with the coordinator after inactivity (no commands sent from coordinator to end device; i.e. on/off) for an extended period of time. I have noticed that 50% of the modules will no longer communicate with the coordinator when I test under these conditions. I verified this when I sent an on/off command to the end devices and they didn't turn on/off. I have found some possible solutions such as, "When device joins Zigbee network but security is not matched with Zigbee network..." and "This restart is usually caused by incorrect security settings." So incorrect security matching/settings may be the cause of my problem, but I am no 100% sure.

So how can I make sure the end device will always have communication with the coordinator, even under an extended period of inactivity?

If it is security, how can I "match security" / "correct security settings"?