Part Number: CC2530-RF4CE
hi
when i have this in coordinator and router
#define NWK_MAX_DEVICE_LIST 10 // Maximum number of devices in the
#define NWK_MAX_ROUTERS 6
mean that up to 10 device and 6 router can be connected to the coordinator and each router with this configuration right?
imagin i have this network
(ZE1)--> (ZR1)--> (ZR2)-->(ZC)
when ZR1 try to register in ZC network will it have device indication in ZC or its just have device indication in ZR2
please help