Other Parts Discussed in Thread: Z-STACK
Hello,
I am getting following error in IAR, can anyone tell me what does it mean?
Error[e16]: Segment ZIGNV_ADDRESS_SPACE (size: 0x3000 align: 0) is too long for segment definition. At least 0x1b3 more bytes needed. The problem occurred
while processing the segment placement command
"-Z(CODE)ZIGNV_ADDRESS_SPACE=_ZIGNV_ADDRESS_SPACE_START-_ZIGNV_ADDRESS_SPACE_END", where at the moment of placement the available
memory ranges were "CODE:7c9b3-7f7ff"
Reserved ranges relevant to this placement:
CODE:7c7a9-7c9b2 BANKED_CODE
CODE:7c9b3-7f7ff ZIGNV_ADDRESS_SPACE
BIT:0-7 BREG
BIT:80-87 SFR_AN
BIT:90-97 SFR_AN
BIT:a8-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:d8-df SFR_AN
Error while running Linker