This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531EMK: ZNP / Z-Stack Monitor

Part Number: CC2531EMK
Other Parts Discussed in Thread: CC2531, Z-STACK

My setup :
  • ZC –> CC2531 / ZNP 1.2.1
  • ZED –> zstack home 1.2.1
  • Z-Stack Monitor and Test API.pdf
 
A ZED is connected to the ZNP.
I can see its nwkaddr, ieee, bind a cluster, simple desc, ...
 
I would like to :
  • parse the data (0-128 bytes) for AF_INCOMING_MSG. Is it documented somewhere ?

Len 1 Specifies the length of the data.

Data 0-128 Contains 0 to 128 bytes of data.

  • read for example, the attribute ModelID, cluster GEN_BASIC for my ZED
 
Thanks for any reply, BR
Nises