This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: cc2650

Part Number: CC2650
Other Parts Discussed in Thread: ENERGIA, CC1350

I notice that the cc1350 launchpad and Sensortag can be used with the Energia development platform. However the CC2650 launchpad is excluded - I believe because of some BLE stack licensing issues. Can someone explain why code for the CC2650 can not be developed using the CC1350 energia development platform. The structure of both chips is very similar, and code can be shared between these simplelink products. It is probably so obvious, but if someone can explain why this cannot be done I can move on to  the more traditional "C" with CCS approach.