1) Send the ZDO_MGMT_LEAVE_REQ command to the device which wanted it to leave the network,In the required parameters, the destination address is set to the device's nwkAddr, and the extAddr is set to device's extAddr. But it always fails ,the status is zdoUnsupported;
2) I tried again, the destination address is set to the coordinator's nwkAddr,the coordinator is the default trust centor,and the extAddr is set to device's extAddr. It is able to perform successfully;
so i have a question about this:
In encrypted network, whether the device can't directly execute the ZDO_MGMT_LEAVE_REQ command ? whether it can only follow the second method to achieve the purpose?