This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Connections with Amazon Echo Plus via Zigbee

Part Number: CC2650
Other Parts Discussed in Thread: Z-STACK, , CC2530, CC-DEBUGGER, CC2531EMK,

Hello

Same Problem here.

In University i have a Project, where i Need to connect a device (on/off light) to the Echo Plus using ZigBee. According to Amazon it is possible with ZigBee HA1.2. I've downloaded the z-stack from TI and switched on the EZ mode. But when i want, that Echo Plus finds devices, it does not find any :(

Can someone help me please? I always thought ZigBee and its Pairing is standardized, but nevertheless it is not that easy...

Regards

Patrick