Part Number: PACKET-SNIFFER
Other Parts Discussed in Thread: CC2531
Good Morning,
I'm starting an RSS analysis study on zigbee networking.
I still have little knowledge in the area.
I bought 5 CC2531 USB Dongle for first:
Learn to communicate with the notebook.
Learn how to create a network.
Learn how to read network data using Python.
So on and on.
I have already received the modules and installed Packet Sniffer as
"CC2531 USB Evaluation Kit Quick Start Guide" Installed version was the 2.18.1 on my Windows 7 64 bit.
When I precede the star (Choosing the IEEE 802.15.4 / ZigBee protocol) in the "Capturing Device" tab I have the recognized CC2531 USB Dongle (USB Device ID = 5235) - CC2531.
On windows in device control, appears Cebal - USB Dongle CC2531.
How to set up simple communication? Which options to select in the other tabs (Radio Configuration, Select Fields, Packet details, Address Book, Display filter, Time line).
In both CC2531 USB Dongle Led 2 is green and is constantly on.
I would greatly appreciate the help.