For example, zigbee device can reporting attribute value to reporting target that has set binding.The maximum of binding target is limited by binding-table size “NWK_MAX_BINDING_ENTRIES”. But once I set “NWK_MAX_BINDING_ENTRIES” more large, and the zigbee device binding more target, will it lose to send message to some one target? If NWK_MAX_BINDING_ENTRIES is more than Z-stack send Buffer?
Where is Z-stack's Binding Send Buffer?NWK Buffer or MAC Buffer(MAC_CFG_TX_DATA_MAX)