Hi,
we're running a Zigbee network with about 30 end devices and 15 routers. End devices cannot join the network at certain routers. They don't connect even though there are two or three other routers around. Other routers iin less packed areas work fine.
Do you have any idea how to fix that? The max broadcast was increased to 128 in the f8wConfig. The other values concerning joining are at default.
Thanks,
Matt