Hello Everyone,
I have recently bought the CC2530DK and want to implement the OAD feature.Though i saw some discussions regarding the same, i couldn't find a clear solution.
I have been folowing the doc swra257-Over air download for CC2530 Soc,but failed in the process.
We are using, CC2530 development kit which consists of 2 smartRF05EB,CC2530EM & CC2531 dongle.
Do i understand it correctly when i say
1.Download Dongle.eww project to the EB which is to be used as Dongle device- ie download Dongle.eww & then run ZportApp application code ?
2.Download boot.eww project to the devices which will recieve OTA upgrade & then OAD enabled application code.
3.Connect the Dongle to PC via serial port and open ZOAD to start OTA?
When i download boot.eww project and then OAD application code it gives me the following error and fails
Warning:Stack Pointer outside Stack segment!
Why is this happening?
I am in desperate need of help and help would be appreciated.