Part Number: CC2538
Hi,
I tested CC2538 with SmartRF06EB.
It is downloaded with SmartRF06EB.
I got a TMS320-XDS100-V3 in Olimex market.
But, I can not download my board.
I tested EWARM 7.40 and TMS320-XDS100-V3.
IAR message is "Fatal error: Failed to connect to the XDS emulator (connect ICEPick)... (Error -182 @ 0x0) The controller has detected a cable break that is near-to itself. The user must connect the
cable/pod to the controller. (Emulation package 7.0.188.0) Session aborted!"
What's the matter?
my environment is the picture.