Part Number: CC2430
Other Parts Discussed in Thread: CC2652R, CC2530
Hi All
Customer would like to add function in their code to check CC2430 flash lock protection bit status. Could you help advice which address to check the data?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The flash lock protection byte is stored at location 0x000 of the flash information page which is located in the lowest 2 KB part of flash. As this part is NRND and not competitively priced I highly recommend that the customer consider migrating to the CC2530 or evaluating the new CC2652R.
Regards,
Ryan