This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2650: ZED Leave network

Part Number: CC2650


Tool/software: TI-RTOS

Hello

I use a CC2650 MCU and i communicate over ZigBee. 

I built a lamp, and when i start the device, i made, that EZ mode automatically starts.  Everything works fine, but now i want, that before EZ mode is started, that my device leaves the known Network. When i switch on my device it Always wants to rejoin the last Network.

I do not want to connect a Debugger every time and clear the Memory.

Is there a function i can call at the beginning, so that every known Network is forgotten?

BR Patrick