Hi Team,
Customer reported an issue that while powered on the CC2538, the current consumption will be increased slowly and then dropped fast to a very low stable current consumption. And this situation also existed while erased full FLASH image at powered on.
Also tried below steps:
1) Connect the RESET_N pin to GND, powered on CC2538, the issue still exist;
2) Using test code, after powered on, using Watchdog to trigger software reset, the issue didn’t exist after software reset;
3) Remove CC2538 from PCB board, test the current consumption of the board, no such issue;
4) Re-work the CC2538 into the board, the issue still exist at power on stage.
Support Need:
This issue seems only exist at the power on stage, could you kindly help to give comments for the power on current consumption issue?