Other Parts Discussed in Thread: Z-STACK, CC2530, CC2530EMK, CC2531EMK, CC-DEBUGGER
Hi to All Team members,
Right now I am using Anaren A2530E24C Zigbee module with preloaded inbuilt ZNP stack version 2.5.1 as a mesh network. Its kind request to you to please give me information for below mentioned queries.
(1) Is Anaren module A2530E24C hsupport of all features of Zigbee PRO 2007. Is this module will have support of Zigbee 3.0 specification?
(2) If Anaren module A2530E24C do not have support of Zigbee 3.0 specification.
(A) Is it posible to implement Zigbee 3.0 specification within same module? If possible what will be the procedure for this?
(B) If it is not possible to implement Zigbee 3.0 specification within same module than which type of module i have to use and also send me link/process to implement Zigbee 3.0 standard.
(3) With Zigbee 3.0 specification support,can all devices communicate with each other in mesh network having different profile like general custom profile, light link and home automation profile?
Thanks and regards,
Ronak Jain