Other Parts Discussed in Thread: Z-STACK, , CC2538, CC2652R
Hello,
I am using Z-Stack HA 3.0.1 with Z-Stack Linux Gateway. Here I am facing a problem where when I try to add new device(complete new/fresh ieee address) to the coordinator using Z-Stack Linux Gateway, my device joins the network and than after few seconds it automatically sends Leave command over the network even if the device is not removed from the network through gateway nor is there any leave send from device though application.
Though if I use some old device(with old ieee address) that sometime back have joined that coordinator but currently is not part of that network and has fresh code in it, the device works perfectly fine i.e. it does not leave the network.
I have attached sniffer data for both the cases, could anyone help me figure out the problem here.