Part Number: CC2530
Hello,
I'm trying to plot the network distribuition in order know which device connects where. To do this I'm trying to use the message "LQI Request" that supposedly gives out this information.
What I found out is most devices with the relationshiop "None of the above" instead of "child" or "parent". At first I assumed this relationship was shown when the device was a neighbour but neither a parent nor a child. The thing is after scanning the entire network some devices don't have parents not allowing me to draw the current network configuration.
I also tried the messages of address discovery, when used with request type extended the reply gives out the neighbours connected to the device but doesn't seem to work for what I need.
Using Ubiqua I can confirm the current device parent is not being reconized in the "LQI Request". Is there a better suited message to do this? The network is composed by devices with the stack 1.2.2a and 3.0.1. All routers and coordinator are in the stack 3.0.1.