Part Number: CC2650
I want to know if there is some guide to use a SmartRF05EB + CC2530DK_EM as a ZigBee Coordinator with the SampleThermostate example and the SampleTemperatureSensor example on the CC2650 LaunchPad, because I can only find the guide for the CC2650 Sensor Tag, and trying to change the configurations I can not start from that example. I want to know if it is possible and (if it is) if there is some guide for the LaunchPad configuration (Like with the SampleSwitch guide that tells what to change from the default code).