This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: Startup network Z-Stack 3.0.1

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK

HI All!

I try  to migrate to Z-Stack 3.0.1 from prevision version and have same qestoin.

The first:

In document "ZNP Inteface specification"   described proceduer of startup Zigbee network.  For  ZC na ZR I must  set two flags Net_Formation and Net_staeering for startup of net. But if i star my  ZR  with both flags(it is the fist switch on!!!) and the ZR not found of ZC (For exaple ZC is swith off)  ZR start and set up new net.  And if after i start my ZC the ZC star normaly (Network Restore) but can not see ZR and ZR don't see ZC too.   Can i start my ZR like ZED  without Net_Formation ? I this case ZR don't setup new network and ZC can strart normaly.

The second:

I start my ZR and it normaly join to ZC.  Then i start the ZED (for exaple it ZED can see ZR but don't see ZC)  Is this  ZED normaly join to ZR ? Or i must Pirmit _Join command on ZR? The security configuration is default.