This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: Smart RF packet sniffer use case

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, CC2530, CC2531,

Hello everyone,

Just a basic question: Can I use Smart RF packet sniffer (not sniiffer 2) to sniff the packets of Lauchxl-cc2650. One the website, cc2650 is written under "can be used to capture packets from". I didn't get it. 

I've CC2530 acting as a coordinator (presently powered by the battery) and launchPad CC2650 as a end device (by USB). I've installed the packet sniffer and under Zigbee/IEEE802.15.4, I am not seeing CC2650 as a supported device. Please advice me Can I use the sniffer agent to trace the data packets? Any good resource will help me a lot.

Thanks in advance. 

Regards,

Priya