This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: Z-Stack and Parent Annce

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK

How I understund from manual of new version of Z-Stack the ZC or ZR send ParentAnnce after start of Stack.

And if same Full Device (FD) get this message it reqest to sender if his table of childs consist specific childs.

After this sender must to clear this child from table. Is it true?

Is this algoritm same for ZR and ZC?

  • After this sender must to clear this child from table. Is it true?

    Yes, it's true.

    Is this algoritm same for ZR and ZC?

    Yes, it's the same.

  • oK!

    I chek today one more times.
    Some days ago I got next:

    Use ZNP and my application based of GenericDevices with MT.

    The EXPERIMENT 1
    Build net on the table ZC, ZR, ZED. ZED join to ZR. switch of router. Check child table of ZC by UTIL_GET_DEVICE_INFO. I can see rejoin ZED to ZC. It is ok. Then I Start router and check child table of ZR by UTIL_GET_DEVICE_INFO. The table is clear.

    The EXPERIMENT 2 (Is mirror to The EXPERIMENT 1)
    I join ZED to ZC. Switch of ZC. ZED join to ZR. Then I Start ZC and check child table of ZR by UTIL_GET_DEVICE_INFO. I can see my ZED in AssocDeviceList. After about 2 minutes the child table of ZC clear..

    In both case I try to moitor by debuger the ZDApp_SendParentAnnce. l This function is call.

    And the weirdness - right now after start ZC the ZC dose'nt answear UTIL_GET_DEVICE_INFO. About few seconds. And answer other command.
  • Hi Pavel,

    Can you detail the exact issue you are experiencing right now? Does it relate to parent announce handling or responding to a UTIL_GET_DEVICE_INFO command? Do you mean that this condition only lasts for a few seconds and are other MT_UTIL commands answered during this time?

    Regards,
    Ryan
  • Do you change anything to ZNP source code when you test this?

  • ok! I repeat experement and write again.