hi to all
i am facing problem regarding building demo project which is downloaded from ti web site
I have done following thing to build my project which is "demo sensor " project
- i have unziped the file that name as "swrc147a" at location "C:\Texas Instruments\ZStack-CC2530-2.3.1-1.4.0\Projects\zstack\Samples"
- then i have opened IAR WORKBENCH .
- Project>>add existing project .
- browse to lacation of project from above path
- then add the project by clicking ok button
- then from Project>>build all
- then message pop up to save project
- then i have save with different name
- then build the project
after building project we have following linking ERRor as follow
Error[e46]: Undefined external "macPib" referred in mac_beacon ( C:\Texas Instruments\ZStack-CC2530-2.3.1-1.4.0\
Projects\zstack\Libraries\TIMAC\bin\TIMAC-CC2530.lib )
Error[e46]: Undefined external "MAC_MlmeSetReq::?relay" referred in mac_beacon ( C:\Texas Instruments\
ZStack-CC2530-2.3.1-1.4.0\Projects\zstack\Libraries\TIMAC\bin\TIMAC-CC2530.lib )
Error[e46]: Undefined external "macPibReset::?relay" referred in mac_beacon ( C:\Texas Instruments\
ZStack-CC2530-2.3.1-1.4.0\Projects\zstack\Libraries\TIMAC\bin\TIMAC-CC2530.lib )
Error[e46]: Undefined external "MAC_MlmeGetReq::?relay" referred in zmac ( C:\Texas Instruments\
ZStack-CC2530-2.3.1-1.4.0\Projects\zstack\Samples\SensorDemo\CC2530DB\SensorEB\Obj\zmac.r51 )
Error while running Linker
I hope ti's esteem user will help in this regards
Thanks
Anubhav